Technical FAQs

Ask a Question

Can the 240 volt 8430 MPS device be used at 208 volts?

Yes, the device can be adjusted from 75 - 100% of the nominal voltage. This gives it a range of 180 to 240 volts.

CTA-ID : 13237
Was this helpful?
What can we do to improve the information ?