Technical FAQs

Ask a Question

What is the speed regulation for the ATV66 drive?

Speed regulation is .5% is available with Tachogenerator feedback, with the optional flux vector module it is 0.01% and typically it is 3% as determined by motor slip.


CTA-ID : 13233
Was this helpful?
What can we do to improve the information ?