Technical FAQs

Ask a Question

What is the wire range of the Main Breaker lug used in a EZM31600CB?

A PAF2036 circuit breaker frame with PA31600RC rating columns is used as the Main Breaker in this device. The line lugs accept (6) 1/0 AWG - 750 kcmil Al/Cu conductors per phase. The same range is provided on the neutral lug.


CTA-ID : 13232
Was this helpful?
What can we do to improve the information ?