Technical FAQs

Ask a Question

What is the wire range of the Main Breaker lug used in a EZM11200CB?

A PAF2026 circuit breaker frame with PA21200RC rating columns is used as the Main Breaker in this device. The line lugs accept (4) 1/0 AWG - 750 kcmil Al/Cu conductors per phase. The same range is provided on the neutral lug.

CTA-ID : 13228
Was this helpful?
What can we do to improve the information ?