Technical FAQs

Ask a Question

What are the repair parts for the H223N series F1? (may be shown as F01)

Issue:
Repair parts

Product Line:
HD SS

Cause:
Maintenance

Resolution:

The repair parts for the H223N, series F1 (F01) are as follows. No other parts are available.

Interior kit - HSIF210F (Includes line & load base assemblies, mechanism, arc suppressor, all mounting hardware and instructions).
Load base kit - HLB210F (includes load base & mounting hardware).
Arc Suppressor kit - HAS0610F - (includes arc suppressor & mounting hardware)
Lug kit - AL10F - (kit includes 6 lugs)
Handle/Mechanism kit- HM0610F (kit includes handle, mechanism, lockplate & mounting hardware)
Neutral Assembly - SN0610 (includes neutral assembly & bonding screw)
Neutral bonding screw - 40283-456-51 (Obsolete - replaced by 40283-656-50)


CTA-ID : 13073
Was this helpful?
What can we do to improve the information ?