Technical FAQs

Ask a Question

What are the repair parts for the HU462AWK, series F3? (may be shown as F03)

The repair parts for the HU462AWK, series F3 (F03) are as follows. No other parts are available.

Interior Kit - HSIU4603606CF (includes line base Assembly, mechanism, arc suppressor, all mtg. hardware and instructions).
Arc Suppressor Kit - HAS0610F- TWO kits required (includes arc suppressor, mtg. hardware and instructions).
Lug Kit - CL0306F - TWO kits required (includes 6-lugs and mtg. hardware).
Handle/Mechanism Kit - HM0610F (includes handle, mechanism, lockplate, gasket, all mtg. hardware and instructions).


CTA-ID : 13070
Was this helpful?
What can we do to improve the information ?