Technical FAQs

Ask a Question

Customer asks if the 9001 KR9RH13 can be converted into an illuminated

Yes, since they both use the 9001 KR9 basic operator. Remove the translucent spacer on the non-illuminated operator and mount a light module.


CTA-ID : 13493
Was this helpful?
What can we do to improve the information ?