Technical FAQs

Ask a Question

What is the wire range of the Main Breaker lug used in a EZM3800CB?

An MHP36800 circuit breaker is used as the Main Breaker in this device. The line lugs accept (3) 3/0 AWG - 500 kcmil Al/Cu conductors per phase. The same range is provided on the neutral lug, but will accept (4) conductors.

CTA-ID : 13226
Was this helpful?
What can we do to improve the information ?