Technical FAQs

Ask a Question

DUPLICATE SEE FA110937 - What is the wire range of the Main Breaker lug used in a EZM3600CB?

THIS IS A DUPLICATE SEE FA110937

An MHP36600 circuit breaker is used as the Main Breaker in this device. The line lugs accept (3) 3/0 AWG - 500 kcmil Al/Cu conductors per phase. The same range is provided on the neutral lug, but will accept (4) conductors.


CTA-ID : 13225
Was this helpful?
What can we do to improve the information ?