Technical FAQs

Ask a Question

Will field-installed electrical accessories change the dimensions of an LA circuit breaker?

No. The field installed accessories are installed internally to the breaker in the same way it is factory installed, and will not change the dimensions.

CTA-ID : 13061
Was this helpful?
What can we do to improve the information ?