Technical FAQs

Ask a Question

Will field installing electrical accessories change the physical dimensions of an MA or MAL circuit breaker? <br />

No. The field installed accessory is installed internally to the breaker in the same way it is factory installed.


CTA-ID : 13060
Was this helpful?
What can we do to improve the information ?