Technical FAQs

Ask a Question

Will field-installed electrical accessories for the PA breaker take up more room than factory-installed devices? <br />

Yes. The field installed accessories are installed on the exterior of the breaker and will change the outline dimensions of the PA PH PE PX PC breakers.

CTA-ID : 13059
Was this helpful?
What can we do to improve the information ?