Technical FAQs

Ask a Question

What are the repair parts for the H321N, series F5? (may be shown as F05)

Issue:
What are the repair parts for the H321N, series F5? (may be shown as F05)

Product Line:
Heavy Duty Safety Switch

Environment:
Replacement parts

Cause:
Maintenance required

Resolution:
The repair parts for the H321N, series F5 (F05) are as follows. No other parts are available.

Line Base Assembly -40566-424-50 (requires one per switch. Arc suppressor assembly not included)
Load Base Assembly - 40566-411-50 (requires one per switch)
Arc Suppressor Assembly - 40560-018-01 (requires one per switch)
Lug Assembly - 40251-016-52 (per lug)
Switch Mechanism - 40566-107-50
Handle Assembly - 4056684150K
Lockplate - 40566-376-01
Neutral Assembly - SN03
Neutral Bonding Screw - 40283-456-51 (Obsolete - replaced by 40283-656-50)


CTA-ID : 12938
Was this helpful?
What can we do to improve the information ?