Technical FAQs

Ask a Question

What is the maximum distance apart the two operators can be when using the 9001K3 interlock mechanism?

The 9001 K3 is adjustable from 1.75 to 2.5 inches, centerline to centerline.


CTA-ID : 13470
Was this helpful?
What can we do to improve the information ?