Technical FAQs

Ask a Question

What is the wire range of the Main Breaker lug used in a EZM1600CBU?

An MHF26600 circuit breaker is used as the Main Breaker in this device. There are no line side lugs provided. The suffix ``U`` of the catalog number indicates that the device meets EUSERC standards. EUSERC requires factory supplied lug landing pads to accept field installed lugs. Lugs should be ordered separately. Refer to catalog 4100CT9801 for further information regarding available lugs.

CTA-ID : 13208
Was this helpful?
What can we do to improve the information ?