Technical FAQs

Ask a Question

What is the coil consumption of the Integral 18?

AC: Inrush: 75 VA at 50 hertz, 90 VA at 60 hertz.
Sealed: 8 VA at 50 hertz, 9 VA at 60 hertz.

DC: Inrush 100 watts, 1.5 watts sealed.


CTA-ID : 12206
Was this helpful?
What can we do to improve the information ?