Technical FAQs

Ask a Question

What are the replacement contacts for a ZCKJ1?

This is a non plug in style device and the contacts are XE2SP2151.

These contacts are silver, rated for 10 amps, with 1 normally opened / 1 normally closed contact, and snap action.


CTA-ID : 12374
Was this helpful?
What can we do to improve the information ?