Technical FAQs

Ask a Question

What are the replacement contacts for a ZCKJ21?

This is a plug in style device and the contacts, and integral cover, are ZCKJ02.

These contacts are silver, rated for 10 amps, with 2 normally opened / 2 normally closed contacts, and snap action.

CTA-ID : 12372
Was this helpful?
What can we do to improve the information ?