Technical FAQs

Ask a Question

9007AB1-S1 - snap switch - does it come with 1NO, 1NC contacts?<br />

Per Raleigh Help file - this is a 9007AO1 with a roller leaf operator. The 9007AO1 is 1NO, 1NC. The S1 changes the roller slightly.

CTA-ID : 12191
Was this helpful?
What can we do to improve the information ?