Technical FAQs

Ask a Question

Does the ATV21 remote keypad store and transfer both the drive configuration ``PLUS`` the BacNet card configuration?

The remote keypad should be able to store and transfer all memory words in the drive, so that will include the Bacnet parameters.

CTA-ID : 2054926
Was this helpful?
What can we do to improve the information ?