Technical FAQs

Ask a Question

How much current does the control circuit of a PAM02 motor operator draw?

30 mA at 120Vac
15 mA at 48Vdc
3 mA at 24Vdc


CTA-ID : 12171
Was this helpful?
What can we do to improve the information ?