Technical FAQs

Ask a Question

What are the repair parts for a H326NAWK Series E2 Heavy Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Complete interior - HN326NAE1 (includes line & load base assembly`s, neutral assembly, arc suppressor assembly, Box insulator, line phase insulators and mounting hardware)
Line base assembly - 40552-214-50 SEL (3-required and arc suppressor assembly is not included)
Load base assembly - 40552-215-50 SEL (3-required)
Arc suppressor assembly - 40512-045-01 (3-required)
Lug assembly - 40256-024-50 (2 required per base assembly)
Neutral assembly - H600SNC
Line base phase insulator - 40512-014-01 (2 required)
Load base phase insulator - 4052-191-01 (2-required)
Line & load base mounting screws - 40206-009-01 (2 required per base assembly)
Handle assembly - 40512-172-50 SEL
Vault handle - 40512-194-50 SEL
Handle knob kit (black & red knob at end of handle) - 44011-427-50
Neutral bonding assembly - 40283-253-50 SEL


CTA-ID : 12482
Was this helpful?
What can we do to improve the information ?