Technical FAQs

Ask a Question

What is the catalog number and availability for a Trilliant GFCI branch breaker, 1 pole, 15 ampere?

Issue:
Product design features

Product Line:
Trilliant Load Centers and branch breakers

Environment:
Branch breaker

Cause:
Application

Resolution:

The catalog number for a 1pole, 15amp Trilliant GFCI branch breaker was SDT115GFI. But this breaker is Obsolete, No longer available with NO replacement. 

CTA-ID : 12470
Was this helpful?
What can we do to improve the information ?