Technical FAQs

Ask a Question

What are the repair parts for a H265 Series E2 and E4 Heavy Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Complete interior - HN265E2 (includes line & load base assemblies, arc suppressor assembly, Box insulator, line & load phase insulators and mounting hardware)
Line base assembly - 40552-188-50 (2-required, arc suppressor assembly not included)
Load base assembly - 40552-190-50 SEL (2-required)
Arc suppressor assembly - 40512-708-50 SEL (2-required)
Lug assembly - 40251-136-50 (1-required per base assembly)
Line base phase insulator - 40512-014-01(1-required)
Load base phase insulator - 40552-191-01 (1-required)
Line and load base mounting screws - 40206-009-01(2-required per base assembly)
Cross arm insulators - Consists of 4 parts: (2) 40552-177-01 (left and right pieces), (1) 40552-178-01 (middle piece) and (1) 40552-157-01 (dust shield ties them together behind the cross arm)
Handle assembly - 40512-172-51
Handle knob kit (black & red knob at end of handle) - Series E2 is 44011-427-50, Series E4 is 40283-435-50
Door thumb screw and retainer - 44050-434-01 & 44050-490-01

CTA-ID : 12325
Was this helpful?
What can we do to improve the information ?