Technical FAQs

Ask a Question

What is the conductor temperature rating for the Main Lugs of a QO load center?

The lugs are suitable for 75 degree C conductors. 90 degree C conductors may be used if installed in accordance with the 2002 NEC (National Electrical Code) Article 110.14(1)(b)(2).

CTA-ID : 12318
Was this helpful?
What can we do to improve the information ?