Technical FAQs

Ask a Question

Are thermal units required for the Class 8536 Type SJ NEMA size 7 starter?

No, this starter is provided with a solid state overload relay which does not require thermal units.


CTA-ID : 12636
Was this helpful?
What can we do to improve the information ?