Technical FAQs

Ask a Question

What is part number for white labels (markers) on front face at bottom of XPSAT? <br /> (These are the labels that the cutomers write-on and pop in and out so they are replaceable).<br /> See Machine Safeguarding 9007CT9702R2/00, pg. 89 for picture of units with markers.

The original is not available as a spare part. Customer can use a LA9D92 as a replacement marker. This is 2mm longer than the original. See Digest 172, pg. 15-11 for proposed replacement``.


CTA-ID : 12147
Was this helpful?
What can we do to improve the information ?