Technical FAQs

Ask a Question

What are the repair parts for a H326 Series E1 and E4 Heavy Duty Safety Switch?

The parts listed here are the only field replaceable parts.
Complete interior - HN326E1 (includes line & load base assembly, arc suppressor assembly, Box insulator, line phase insulators and mounting hardware)
Line base assembly - 40552-185-50 SEL (3-required and arc suppressor assembly is not included)
Load base assembly - 40552-187-50 SEL (3-required)
Arc suppressor assembly - 40512-045-01 (3-required)
Lug assembly - 44050-446-01 (2 required per base assembly)
Line base phase insulator - 40512-014-01 (2 required)
Load base phase insulator - 40552-191-01 (2 required)
Line & load base mounting screws - 40206-009-01 (2 required per base assembly)
Handle assembly - 40512-172-50 SEL
Door thumb retainer - 44050-490-01
Door thumb screw - 44050-434-01
Handle knob kit (black & red knob at end of handle) - Series E1 is 44011-427-50, Series E4 is 40283-435-50


CTA-ID : 12431
Was this helpful?
What can we do to improve the information ?