Technical FAQs

Ask a Question

Are the control operators maintained or momentary on the Class 2510 manual devices?

All manual controllers provide maintained contacts. The now obsolete low voltage protection devices also used maintained operators but were tripped via internal voltage sensing coil.

CTA-ID : 12286
Was this helpful?
What can we do to improve the information ?