Technical FAQs

Ask a Question

What Class of fuse does the H362WH and H362AWH safety switch accept?

Issue:
Selection/Application

Product Line:
HD SS

Cause:
Fuse Selection

Resolution:
These switches accept Class H, K or R fuses as standard.  With Class H, K or R fuses installed, the switches are UL listed for use on systems with up to 10,000 RMS Symmetrical Amperes available fault current.
NOTE: DO NOT USE RENEWABLE LINK FUSES IN SQUARE D SAFETY SWITCHES. The use of renewable link fuses may adversely affect user safety, impair reliability and will void the warranty.


CTA-ID : 12427
Was this helpful?
What can we do to improve the information ?