Technical FAQs

Ask a Question

Do we still make QO320D cb`s?

No. The QO320D is a ``Delta`` breaker. Two phases are obtained from the single phase panel where it resides. The third phase is obtained by wiring the third pole to an external third phase. A typical application would be a single phase lighting panel with one circuit needed for a three phase motor.

CTA-ID : 12270
Was this helpful?
What can we do to improve the information ?