Technical FAQs

Ask a Question

Can you field reverse a 9037HG type float switch?

Yes it can be field modified. Refer to 9037 HG service bulletin 65013-013-90B or 9038-893 for instructions on field reversing.


CTA-ID : 12269
Was this helpful?
What can we do to improve the information ?