Technical FAQs

Ask a Question

Is 415 volt replacement control coil available for LC1D2501?

Yes, order LX1D4N5 for 50 hertz or LX1D4N7 for 50/60 hertz. Average coil consumption is 90 VA inrush 7.5 VA sealed for 50 hertz, 1000 VA inrush 8.5 VA sealed for 60 hertz and 100 VA inrush 8.5 VA sealed for 50/60 hertz.


CTA-ID : 11394
Was this helpful?
What can we do to improve the information ?