Technical FAQs

Ask a Question

9007C54K What type of material is the wobble stick made of ?<br />

It is a spring steel material.



CTA-ID : 12011
Was this helpful?
What can we do to improve the information ?