Technical FAQs

Ask a Question

9007C86B2 - Is the pretravel 10 or 13 degrees?<br />

It is 13 for this limit switch (due to reed contacts) but the same head on a C66B2 limit switch body (standard contacts) would be 10 degrees.



CTA-ID : 11979
Was this helpful?
What can we do to improve the information ?