Technical FAQs

Ask a Question

9007CR explosion proof. Are the contacts sealed?<br />

No, the enclosure is designed to contain an explosion within it so it doesn`t escape into the potentially hazardous atmosphere.



CTA-ID : 11970
Was this helpful?
What can we do to improve the information ?