Technical FAQs

Ask a Question

9007C54B Customer has this limit switch with the following Forms: D5, T, Y35, and Y140. Can you identify these Forms?<br />

This is a special configuration for Chrysler, uses a Viton seal, a 5 pin microconnector, and tamper proof screws. Only form Y140 can be ordered separately.



CTA-ID : 11965
Was this helpful?
What can we do to improve the information ?