Technical FAQs

Ask a Question

What Class of fuse does the H365, H365N, H365R, H365NR, H365DS, H365NDS, H365AWK and H365NAWK, Heavy duty safety switches accept?

Issue:
Product design features

Product line:
Heavy Duty Safety Switches

Environment:
Fuse Class

Cause:
Application

Resolution:
These switches accept Class H or K fuses as standard. Options include Class R fuses (field install Class R Fuse Kit HRK4060) and Class J fuses (field relocate the fuse base assembly to alternate position marked in the enclosure). With Class H or K fuses installed, the switches are UL listed for use on systems with up to 10,000 RMS Symmetrical Amperes available fault current. With Class R fuses (and HRK4060 fuse kit installed) or Class J fuses installed, the switches are UL listed for use on systems with up to 200,000 RMS Symmetrical Amperes available fault current.

NOTE: DO NOT USE RENEWABLE LINK FUSES IN SQUARE D SAFETY SWITCHES. The use of renewable link fuses may adversely affect user safety, impair reliability and will void the warranty.

CTA-ID : 11741
Was this helpful?
What can we do to improve the information ?