Technical FAQs

Ask a Question

What Class of fuse does the H325, H325N, H325R, H325NR, H325DS, H325NDS, H325AWK and H325NAWK heavy duty safety switches accept?

Issue:
Product design features

Product line:
Heavy Duty Safety Switches

Environment:
Fuse Class

Cause:
Application

Resolution:

These switches accept Class H or K fuses as standard. Options include Class R fuses (field install Class R Fuse Kit HRK4060) and Class J fuses (field relocate the fuse base assembly to alternate position marked in the enclosure). With Class H or K fuses installed, the switches are UL listed for use on systems with up to 10,000 RMS Symmetrical Amperes available fault current. With Class R fuses (and HRK4060 fuse kit installed) or Class J fuses installed, the switches are UL listed for use on systems with up to 200,000 RMS Symmetrical Amperes available fault current.


NOTE: DO NOT USE RENEWABLE LINK FUSES IN SQUARE D SAFETY SWITCHES. The use of renewable link fuses may adversely affect user safety, impair reliability and will void the warranty.

CTA-ID : 11739
Was this helpful?
What can we do to improve the information ?