Technical FAQs

Ask a Question

9007C54L - Can a maintained contact head be used on the 9007C54L body?<br />

If the desire is a wobble stick with maintained contacts, there is no direct substitute head for this device. If, however, the user will accept a wobble stick type lever arm, for instance, 9007FA1 on page 19-10 of Digest 172, then substitute the 9007C head and use the same body.



CTA-ID : 11961
Was this helpful?
What can we do to improve the information ?