Technical FAQs

Ask a Question

Can fusible Heavy Duty Safety Switches be applied at 50 Hertz (Hz)?

Issue:
Product Features

Product Line:
Heavy Duty Safety Switches

Environment:
Voltage System

Cause:
Application

Resolution:
Yes, 50/60 Hz is standard for all the Heavy Duty Fusible Safety Switches. Contact the fuse manufacturer to determine how to select fuses for 50 Hz applications.


CTA-ID : 11555
Was this helpful?
What can we do to improve the information ?