Technical FAQs

Ask a Question

9007C54B2 Customer is asking if this device is oil tight.<br />

Yes. It is rated NEMA 13 which protects against spraying of non-corrosive oils..



CTA-ID : 11935
Was this helpful?
What can we do to improve the information ?