Technical FAQs

Ask a Question

9007 Type C - If a form Y1851 is selected will the limit switch still maintain the NEMA 6P rating?<br />

This form (epoxy filled) will not effect the NEMA rating, the limit switch will still have a type 6P rating. Note: epoxy only fills the lower end of the enclosure, unlike competitors which totally fill the electrical wiring area



CTA-ID : 11924
Was this helpful?
What can we do to improve the information ?