Technical FAQs

Ask a Question

Can you get a 9007MS or ML with 2 - normally open sets of contacts - and having a neutral position? <br /><br /><br /><br /><br />

Cannot get the mini 9007 MS or ML with 2 normally open contacts and a neutral position?

Alternate would be the 9007C68T10. Digest 172, pg. 19-4.


CTA-ID : 11903
Was this helpful?
What can we do to improve the information ?