Technical FAQs

Ask a Question

Why isn`t the CQRB200 available to wholesale distributors?

This is a Retail Products Division product only. It is equivalent to C200RB with a QOM2200VH field installed, which is available through the wholesale distributor market. The wholesale distributor has the ability to provide any QOM2---VH breaker, 100-200 ampere, for the C200RB Meter Main device, a flexibility required to service the contractor trade.


CTA-ID : 11863
Was this helpful?
What can we do to improve the information ?