Technical FAQs

Ask a Question

9007 A016 open type limit switch. What box does it go into?<br />

The 9007 A016 is an open switch which can be used as an assembled replacment for an installed 9007 AW16 Box must be reused as it is sold only as part of 9007AW16.

CTA-ID : 12076
Was this helpful?
What can we do to improve the information ?