Technical FAQs

Ask a Question

Is it possible to identify the 9007C54CS17?<br />

The limit switch uses a modified head and body for low temperature operation. There is no substitute for this device. It is configured with the S9 hub for a larger diameter lever arm from the T and FT line.


CTA-ID : 12070
Was this helpful?
What can we do to improve the information ?