Technical FAQs

Ask a Question

9007 Neutral Position Limit Switch, how do contacts change state when going both directions?<br />

9007C68T10 has 2 sets of NO/NC contacts. Only 1 set of NO and 1 NC change state when moving off neutral. One set responds to CW movement, while the other set remains at rest. When the lever returns to neutral, all contacts are at their at rest positions. When CCW movement occurs, the second set of NO/NC contacts change state while the first set remains at rest. Again, return to neutral, all contacts return to their at-rest positions.


CTA-ID : 12064
Was this helpful?
What can we do to improve the information ?