Technical FAQs

Ask a Question

9007C54B2 and 9007C68T10 - are these the same size? same operation?<br />

Both are the same size, but operation is very different. 9007C54B2 has 1NO/1NC contact; contacts change state when arm moves either CW or CCW. 9007C68T10 has 2NO/2NC with neutral position. 1 pair changes state w;hen going CW, the other pair changes state when going CCW.



CTA-ID : 12056
Was this helpful?
What can we do to improve the information ?