Technical FAQs

Ask a Question

9007C style limit switch can you add a 9007FA3 12` spring rod to an existing lever to make it longer?<br />

No, you can install one lever arm per switch. If the specials are not long enough, you can use the 9007R16 or R17 levers and add either the rod or keystock in any length you desire to complete a lever. These two devices require the 9007S9 hub to fit them to the 9007C limit switch.

CTA-ID : 12030
Was this helpful?
What can we do to improve the information ?